AnsweredAssumed Answered

Input resolution of 3840*2160@30 for ADV7619

Question asked by Jacky-zheng on Aug 16, 2016
Latest reply on Sep 6, 2016 by JeyasudhaMuthuPerumal

Hello,

ADV7619 can support 4K*2K@30 resolution video input,I see this information in the datasheet(page 7 of UG-237):

The ADV7619 incorporates a dual input HDMI receiver that supports all mandatory 3D TV formats defined in HDMI 1.4a specification, HDTV formats up to 1080p deep color 12-bit per channel or 2160p8bit color per channel and display resolutions up to 4k by 2k (3840 x 2160 at 30 Hz).

Must I input the 3840 x 2160 at 30 Hz video with dual input to ADV7619?Can ADV7619 support 3840 x 2160 at 30 Hz(RGB444) video by port A only?And must set PRIM_MODE[3:0] (IO map,Address 0x01[3:0]) to 0110(HDMI-GR)?

BR

Tom

Outcomes