AnsweredAssumed Answered

6GSPS DDS with internal Sweep Capability

Question asked by AMKoosh on Aug 15, 2016
Latest reply on Sep 6, 2016 by JLKeip

Hi,

I’m looking for a 6GSPS DDS with internal sweep capability.

In Direct Digital Synthesizer category at analog.com, the maximum clock frequency is 3.5GHz.Also, there is AD9164 in DAC category, which has a clock rate of 6GSPS. According to AD9164 datasheet, it can be used in NCO Only mode as a DDS. However, it lacks the internal sweep capability.

Does Analog Devices intends to release a DDS with 6GSPS update rate in near future? (3 to 4 months)

 

Thanks in advance

Outcomes