AnsweredAssumed Answered

ADV7619: Free-Run, HS, VS, VCLK

Question asked by A_Wild on Aug 15, 2016
Latest reply on Aug 19, 2016 by GuenterL

Is there a way to completely disable Free-Run via script?

At the moment, even though Free Run is diabled I do get a signal on HS, VS and VCLK.

 

In an other topic I read that you recommend to try tweaking the tri-state of those Outputs. I don't want them to be disabled when still connected to a HDMI-Source. Those Pins only shall be inactive when no Source is connected.

 

Also the output of HS, VS & VCLK are close to being the same to the values of those ports when there is a HDMI-input.

Outcomes