AnsweredAssumed Answered

absolute maximum input voltage

Question asked by mattholland on Aug 12, 2016
Latest reply on Aug 17, 2016 by mattholland

Table 28 in the data sheet states that input voltages as high as 3.6V are fine as long as VDD_EXT is within specifications. This seems to imply that driving a GPIO above VDD_EXT is not a problem, for example if VDD_EXT is 1.8V, a GPIO can be driven to 2.5V with no danger of forward biasing protection diodes etc. Is this really the case?

Outcomes