AnsweredAssumed Answered

Why do not the adm3485?

Question asked by Skupov93 on Aug 11, 2016
Latest reply on Aug 11, 2016 by Skupov93


Hello!

It is necessary to connect the device(master) to a single sensor(salve), but device(master) have adm3485 and single sensor(slave) have adm485. When there is a transfer from the master to the slave, the data is successfully reach.When there is a transfer from slave to the master, master can not count the data. The oscilloscope shown that after adm3485 a logic zero at the level 1.4 V. Why is this happening?

Outcomes