AnsweredAssumed Answered

ADF4108S

Question asked by ceceille on Aug 3, 2016
Latest reply on Aug 9, 2016 by Brigid.Duggan

Hi all,

 

I am currently looking for a complete PLL for a space application and the phase comparator ADF4108S may be a good option.

On the main page of the component, the discussion section refers to the ADF4108, is it the equivalent of the ADF4108 in a non space qualified range? If yes, it means that I could use the eval board of the ADF4108 in order to test it with my component but would it be possible to change the VCO on the board to have a 6GHz output and a 3GHz on the output devided by 2?

On the board, what are the SMA connector Vtune and VVco used for?

 

Thanks in advance

Outcomes