AnsweredAssumed Answered

two adau1701 in serial mode with controller

Question asked by vasilius on Aug 3, 2016
Latest reply on Aug 15, 2016 by DaveThib

Hello

Now works fine for such a scheme:

 

now1.jpg

 

But i want to use one more ADAU1701, and instead ADC input use digital input and dsp power of second dsp :

 

will1.jpg

 

audio path:

1 analog  in to adc IC1 and after go to digi Out

2 from IC1 digi Out goes to IC2 digi IN and after go to digi OUT for stm32

3 from digi OUT IC2 to STM32 and after back from stm32

4 from STM32 back to IC2 for DAC

5 out to analog from DAC IC2

 

The main difference from my working schema in using another ADAU instead ADC IN, and clock it with I2S LCRK+BCLK from STM32.

The MCLK go from stm32 to both ADAU. 

 

IC3 master

IC2 slave

The main doubt in IC1 - if IC1 is slave and IC2 and clocked both by stm32 - can IC1 send and IC2 recieve directly?

 

Thank yo to answer

Outcomes