AnsweredAssumed Answered

RSSI Measurements

Question asked by Shahid_DE Employee on Aug 2, 2016
Latest reply on Aug 10, 2016 by Shahid_DE

Hello,

I performed RSSI measurements on AD-FMCOMMS3-EBZ board over frequency (800 MHz to 2.4 GHz) and dynamic range with an overall good accuracy. But in some points I have reached a much more precise result with setting the gain manually (in most cases lower than auto gain setting). I think that could be tuned via thresholds?

 

Another point is the actual very high third order harmonic while generating a test tone (both via the GUI and FPGA).

I have seen values up to 10dBc.

Is there a way to improve the auto calibration values with additional manual calibration steps?

 

Waiting for your kind reply.

 

Br

SI

Outcomes