AnsweredAssumed Answered

FMCDAQ2 Input conditioning and signal processing

Question asked by SDR on Aug 2, 2016
Latest reply on Aug 16, 2016 by charlyelkhoury

Hi All,

We have ordered the "Xilinx Kintex® UltraScale™ FPGA DSP Development Kit with JESD204B High-Speed Analog" which contains the FMCDAQ2 board.

The signal we want to process has a bandwith of 200 MHz and is located around 700 MHz.

The signal strength can vary between -10 to -60 dbm.

1. Do we need to place an Input Conditioning board (AGC) in front of the FMCDAQ2?

2. Which DDC configurations/ Sampling Rate would you recommend to process the signal. (So the FPGA could process the high bandwidt data)

 

Thanks in advance.

 

Outcomes