AnsweredAssumed Answered

How to amplifying small signal to high voltage

Question asked by max++ on Jul 29, 2016
Latest reply on Aug 1, 2016 by iamPhil

I'd like to generate the transient in power line system from D/A as image below.

 

Transient.jpg

 

There are 2 points that I want to know including.

1. How to amplifying small signal from D/A to very high voltage 220V?

2. How can I accomplish the rise/fall time of such  level (more than 500V)?

 

This signal is just voltage based supply to power analyzer. It is not drive to actual load anymore.

 

Please guide me to design this amplifier and appreciate if anyone can advise what are the devices that I should use in this design?

 

Thank in advance.

 

Outcomes