AnsweredAssumed Answered

the max bandwidth of AD9361

Question asked by z.q on Jul 25, 2016
Latest reply on Jul 26, 2016 by padmaram

Hi,

There is a question about the max bandwidth of AD9361.

According to UG570, the max baseband channel bandwidh is 20MHz.

If i tried to  use the max baseband channnel bandwidth,the sampling rate must be configured as 61.44MHz?

If I tried to use the max baseband channnel bandwidth and set the sampling rate as 41Mhz,could it happen?

 

Thand you.

Outcomes