AnsweredAssumed Answered

Some basic AD9361 questions: ADC & DMA

Question asked by Stanoneal on Jul 25, 2016
Latest reply on Jul 25, 2016 by CsomI


Hi,

 

A few basic questions about AD9361/FMCOMMS2:

1) Is the ADC linked directly to the DDR via the ADC_DMAC?

2) If I want to add a FFT IP, how should I interface with the ADC, since the FFT core uses AXI stream?

3) Can the control flow of the FFT completely based in the FPGA/PL? Or do I need the CPU/PS to control the flow?

 

fmcomms2_qns.jpg

Outcomes