AnsweredAssumed Answered

ADV7180 Evlauation Kit with MC-495 Camera

Question asked by ganesan31 on Jul 22, 2016
Latest reply on Jul 28, 2016 by JeyasudhaMuthuPerumal

Hi there,

 

I am trying to use the ADV7180-32EBZ eval kit to decode analog video from MC-495 CMOS Image sensor into 8 Bit parallel data to connect to the i.MX6 applications processor. The end goal is to connect this to a display of some sort.

 

As a first step, I connected the camera straight to an analog input on an old TV, and I was able to see the stream.

 

When I use the ADV7180-ADV7392 bridge from A-D and then D-A (the eval kit has two RCA phono jacks that convert analog to digital and then back to analog) and then connect back to the display, I am not seeing the stream from camera.

 

The clocks are fine at 28 MHz and all the voltage supplies are fine. The camera outputs NTSC/PAL at ~525TVL.

 

Am I missing something here? Any inputs would be highly appreciated.

 

Thanks,

Ganesan

Outcomes