AnsweredAssumed Answered

Cross complie question

Question asked by phaedrus on Jul 22, 2016
Latest reply on Jul 22, 2016 by phaedrus

Hello Support.

 

I have developed an application on the AD1940 demo board which works very well. However, I have now realised (with 20/20 hindsight) that the application would have been better developed on the ADAU1701 platform because I would like the target product to run in self-boot mode.

 

I realise that - for various reasons - the application I developed may not run on the ADAU1701 with less RAM, no hardware slew etc.

 

I am now at board layout stage at which point I obviously have to commit to the device type. Is there any statistics that I can access from the design in SigmaStudio which will tell me if the application will run on the ADAU1701? Obviously, I can buy the EVAL-board for the ADAU1701 and test this. But I wonder if there is a way to know this without doing that.

 

Many thanks.

 

Richard

Outcomes