AnsweredAssumed Answered

AD7961 Reference help

Question asked by zynqmedical on Jul 21, 2016
Latest reply on Jul 25, 2016 by AdrianC

Hello,

 

I have been working on using the AD7961 A/D on the Zedboard (Using Zynq Chip) and have come across some errors I cannot figure out.

 

I am using the reference design from analog's wiki page

https://wiki.analog.com/resources/fpga/xilinx/fmc/ad7961

 

I managed to create an IP inside Vivado with matching ports in reference to the reference design. I'm using the the same hardware and software code that was provided.

 

When I try to run the software from SDK the processor goes into an unknown state. This error happens when the software begins to read the Data from the DMA core inside the ADC IP.

 

 

Error happens during this part of the code

 

      // program the DMA module in the ADC core

      Xil_Out32((CF_BASEADDR + 0x040), 0x1); // Power up the core

      Xil_Out32((CF_BASEADDR + 0x088), 0x7); // Reset overflows

      Xil_Out32((CF_BASEADDR + 0x080), 0x0); // DMA stop

 

      Xil_Out32((CF_BASEADDR + 0x084), size * 4 );  // Program the number of bytes to be captured

      Xil_Out32((CF_BASEADDR + 0x080), 0x1); // Start capturing data

 

Do you know of any reason why this is happening?

 

Also, am I able to use the same hardware and software code for the zynq chip instead of the microblaze? The reference design uses Microblaze.

 

Any information would be greatly appreciated!

 

Thank you in advance,

Outcomes