AnsweredAssumed Answered

Setting up the AD9161

Question asked by Hunter101 on Jul 21, 2016
Latest reply on Jul 26, 2016 by danf

Questions about the AD9161 DAC:

 

1. I know what the SPI clock rate is because it is in the data sheet but what is the maximum input clock rate for the AD9161?  I am running 12G data into the DAC.

 

2.  How many registers do I have to program in the DAC?

 

3.  I want the most significant bit to go in first.  I think that is the default in register 0X000.  Is this a correct assumption?

 

3.  I only need one SERDES lane.  I wrote my code to the 0x201 register.  The data I input is hex 20180 to use SERDES lane 7.  Is this correct?

 

Please respond.

 

Randy Draper

Outcomes