AnsweredAssumed Answered

BF704 and ICE-1000

Question asked by Yeti on Jul 21, 2016
Latest reply on Aug 4, 2016 by Yeti

Hi!
I'm using custom board with bf704 and ICE-1000 emulator.

All jtag tests are successful. But when i'm working in CCES 2.3  getting the following error messages:

 

" Attempting to connect to an unknown device, however session is for a ADSP-BF704."

"Error in launch sequence [TpsdkServer] Failed to halt processor 0"

 

I checked all the power supply voltage, checked a quartz resonator signal.

 

i'm using 14-pin connector with the following signals:

14-pin.png

 

What can lead to this error?

Thanks.

Outcomes