AnsweredAssumed Answered

Supported Sample Rates of ad9361

Question asked by sfurman94 on Jul 19, 2016
Latest reply on Jul 20, 2016 by tlili
Branched to a new discussion

Hello,

 

I was wondering what the supported sample rates of the ad9361 are. I have a program that I am running on the Zedboard that is adapted from the libiio stream example. I tried to adjust the sample rate to 200 kHz as opposed to the 2.5 MHz used in the example and I received the error: "Error -22 writing to channel "sampling_frequency" ".

 

Thanks in advance,

Sean

Outcomes