AnsweredAssumed Answered

AD9361 fcomms2 project block design error

Question asked by KolosKoblasz on Jul 19, 2016
Latest reply on Jul 19, 2016 by KolosKoblasz

Greatings everyone!

 

I am trying to reproduce the ZED board ,fmcomms2 example with Vivado 2015.2 using the proper hdl git repo.

I am following the instructions found here: ADI Reference Designs HDL User Guide [Analog Devices Wiki]

I have built every single IP that had suitable .tcl file. It was painful, but seemingly worked.

When I try to run the system_project.tcl in projects/fmcomms2/zed directory the block design gets lots of IP-s, but it terminates with this error:

 

### ad_cpu_interconnect 0x7C400000 axi_ad9361_adc_dma

connect_bd_net -net /sys_cpu_clk /axi_cpu_interconnect/M08_ACLK

connect_bd_net -net /sys_cpu_clk /axi_ad9361_adc_dma/m_dest_axi_aclk

connect_bd_net -net /sys_cpu_resetn /axi_cpu_interconnect/M08_ARESETN

connect_bd_net -net /sys_cpu_resetn /axi_ad9361_adc_dma/m_dest_axi_aresetn

connect_bd_intf_net /axi_cpu_interconnect/M08_AXI /axi_ad9361_adc_dma/s_axi /axi_ad9361_adc_dma/m_dest_axi

ERROR: [BD 5-110] Interface Pin or Interface Port /axi_ad9361_adc_dma/s_axi /axi_ad9361_adc_dma/m_dest_axi not found.

ERROR: [Common 17-39] 'connect_bd_intf_net' failed due to earlier errors.

 

    while executing

"connect_bd_intf_net $m_name_1 $m_name_2"

    invoked from within

"if {[get_property CLASS $m_name_1] eq "bd_intf_pin"} {

    puts "connect_bd_intf_net $m_name_1 $m_name_2"

    connect_bd_intf_net $m_name_1 $m_name_2

..."

    (procedure "ad_connect" line 41)

    invoked from within

"ad_connect axi_cpu_interconnect/${i_str}_AXI ${p_intf}"

    (procedure "ad_cpu_interconnect" line 65)

    invoked from within

"ad_cpu_interconnect 0x7C400000 axi_ad9361_adc_dma"

    (file "../common/fmcomms2_bd.tcl" line 155)

 

    while executing

"source ../common/fmcomms2_bd.tcl"

    (file "system_bd.tcl" line 4)

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 97)

    invoked from within

"adi_project_create fmcomms2_zed"

    (file "./system_project.tcl" line 6)

 

 

 

Please help me because I am on the verge of a nervous breakdown thanks to the AD9361

 

Kolos

Outcomes