AnsweredAssumed Answered

Query about AD9963's TX interface

Question asked by jhshin on Jul 19, 2016
Latest reply on Jul 29, 2016 by larrywelchusa

Hi,

 

My customer is confused the digital interface of AD9963 under the following conditions.

  - CLKP : Single-Ended 1.8V CMOS 16MHz

  - HALF-DUPLEX MODE & one-clcok mode

  - powers down DLL block

  - 0x30 = 0x3E / 0x31 = 0xA7 / 0x3F = 0x00

What is the direction of TRXD, TRXIQ and TRXCLK in the above conditions?

Could you please provice the port timing diagram for TRXD, TRXIQ and TRXCLK ?

 

Thanks in advance.

Outcomes