AnsweredAssumed Answered

ADuC7061 Timer0 external input

Question asked by B.B on Jul 19, 2016
Latest reply on Jul 25, 2016 by MMA

From ADuC7060_7061.pdf (p.67): "The prescaler source can be the low power 32.768 kHz oscillator, the core clock, or from one of two external GPIOs." I found one at P1.0. Where is another? I can't use P1.0 because it is UART Rx pin too.

Outcomes