AnsweredAssumed Answered

ADXL193 Self Test

Question asked by bmalone on Jul 18, 2016
Latest reply on Jul 21, 2016 by bmalone

The data sheet for the ADXL193 describes the self test function: "Activating self-test causes a step function force to be applied to the sensor, while the capacitive coupling term is canceled. The ADXL193 has improved self-test functionality, including excellent transient response and high speed switching capability. Arbitrary force waveforms can be applied to the sensor by modulating the self-test input, such as test signals to measure the system frequency response, or even crash signals to verify algorithms within the limits of the self-test swing." Am I understanding this properly that a known input signal can be applied to the ST pin and the accelerometer's actual response that would be proportional to a real-world acceleration will be output? The existing circuit has this pin connected to a MPU port that is not used. I would like to inquiry our EEs to consider using the ST if operates in the mode I am interpreting. We are using the AD 22282 version. Thanks!

Outcomes