AnsweredAssumed Answered

ADXL193 - Output issue

Question asked by bmalone on Jul 18, 2016
Latest reply on Jul 21, 2016 by bmalone

We sometimes see the output from the ADXL193 that is used in our devices have a 'sticky/notchy' output signal. The environment acceleration range is between 90g - 70g with a smoothly changing value but the accelerometer output is sticking at around 73 g then will spring up/release to properly output/track the environment. This behavior seems to clear when power is completely removed from the circuit. Only some components exhibit this issue. Our EEs do not see an issue with any specific circuit board. Any insight available? Thanks!

Outcomes