AnsweredAssumed Answered

ADP2360 max output current

Question asked by hunl Employee on Jul 18, 2016
Latest reply on Jul 31, 2016 by Migs

Hello,

 

in the datasheet of ADP2360 it is written "the max output current is slightly less than half of peak current IPEAK(through inductor)".

When I check the specs at p. 3 I see I peak is >=126mA (for 0 Ohm), whereas by table 5 at p.12 140mA.

Assuming worst case 126mA; can the part still supply 60mA its output?

 

What is the real limiting factor here?

 

Thanks for any help.

Outcomes