AnsweredAssumed Answered

What is "FrameCapture_ClassDriver_ASX340" project can do ?

Question asked by hiloshi on Jul 18, 2016
Latest reply on Jul 19, 2016 by npai2

Dear Sirs,

I am very new to ADI image sensor solution, I just get a BLIP2 EVM and I am eager to learn something from this board.

I download "ADZS_BF707_BLIP2_Board-Rel1.0.0" and import "FrameCapture_ClassDriver_ASX340" project from Help->Browse Example and run. I have two questions:

1. I expect this project may generate a picture into SD card, however I see nothing inside SD card, why ?

2. When I into debug mode, in the console screen it shows:

Loading application: "C:\Users\julian\cces\2.3.0\examples\bf707_blip2_1.0.0\FrameCapture_ClassDriver_ASX340\Debug\FrameCapture_ClassDriver_ASX340.dxe"

Load complete.

Core clock:      384000000 Hz

System clock:    192000000 Hz

System clock 0:   96000000 Hz

System clock 1:  192000000 Hz

VGA 640x480 @ 30FPS

Then after few seconds, it shows below error message:

A non-recoverable error or exception has occurred.

  Description:   An instruction CPLB miss has occurred without a corresponding CPLB entry.

  General Type:  RunTimeError

  Specific Type: ICPLBMissWithoutReplacement

  Error PC:      0x00000000

 

How to correct it ?

Outcomes