AnsweredAssumed Answered

ADV7391 SD Non Interlaced

Question asked by Jayar@m_423 on Jul 17, 2016
Latest reply on Jul 18, 2016 by JeyasudhaMuthuPerumal

Hi,

 

I'm trying to give the progressive inputs to the ADV7391 in Master mode I have configured the ADV7391 in SD Non Interlaced Mode by setting  1st bit of 0x88 register.The HSYNC and VSYNC are same for both SD interlaced and SD Non Interlaced  in master mode.

 

so please suggest me the input standards that I need to fallow for SD Non Interlaced in Master Mode.

 

Input:

640X480,8bit monochrome,50Hz

Clock In is 27MHz

 

Thanks,

Jayaram

Outcomes