AnsweredAssumed Answered

Problem with output of AD9649 Evaluation Board

Question asked by kinyau94 on Jul 15, 2016
Latest reply on Jul 19, 2016 by DougI


I have a AD9649 Evaluation Board and I have read through the user guide EVALUATING THE AD9266/AD9649/AD9629/AD9609 ANALOG-TO-DIGITAL CONVERTERS [Analog Devices Wiki] , I am trying to get the ADC 2 complement output by standalone mode (without the SPI communication).

I have set the Jumper as shown below:

J203: Pin 1 to Pin 2 (MODE_OR to LED)

J302: Pin 8 No Jumper  (Standalone mode)

          Pin 2 No Jumper (Default Mode)

          Pin 5 to Pin 6 (2's Complement)

J605: Pin 1 to pin 2 ( internal oscillator)

J201 : Pin 2 to Pin 3 (internal 1V reference)

J202: No jumper.

I have tested by input 1V to the input_A, I should expecting "01 1111 1111 1111", but what I get is fluctuating random numbers range from negatives to positive (majorly negative numbers).

Can anyone give some guide on how to setup  standalone mode for  AD9649 Evaluation board?

Thank you!

Outcomes