AnsweredAssumed Answered

Does ADP5062 UVLO disable ISO FET if Vin=0?

Question asked by MBrookes on Jul 15, 2016
Latest reply on Jul 18, 2016 by Leo_Liu

1.  If Vin=0 (USB unplugged) and Bat_Sns drops below UVLO threshold, does the battery isolation FET turn off (Iso_Sx = 0V)?

 

2.  If all I2C registers are at default values, specifically Sys_En control = 00, and USB 5V is connected to Vin, will SYS_EN be pulled low regardless of battery state of charge?

Outcomes