AnsweredAssumed Answered

No rule to make target

Question asked by kschin on Jul 13, 2016
Latest reply on Oct 7, 2016 by Kader.M

after i installed the VisualDSP++, i compiled the project and i encountered the following error:

 

----------------Configuration: mdm_lwip - Release----------------

C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\gmake-378: *** No rule to make target `liblan8700bf527.dlb', needed by `Release/mdm_lwip.dxe'.  Stop.

No valid command(s) to build.

Build was unsuccessful.

 

--------------------------------------------------------------------------------------

the project itself is supposed to be able to compile, i tried to change the Project Options->LDF Settings, so that the .ldf file can be updated to the latest directory path. But the problem still existed.

 

This project can be compiled from other PC, it only this PC encountered this problem, is there any other setting i need to do to solve the problem?

Outcomes