AnsweredAssumed Answered

AD9601

Question asked by dgardner27 on Aug 1, 2011
Latest reply on Aug 17, 2011 by David.Buchanan

For the AD9601, I do not see a specification on maximum currents at the analog inputs. (VIN+, VIN-).

 

Is it safe to assume a 10 mA maximum because of input protection diodes ? I want to protect in case of an over range input signal.

 

I'm doing single ended to differential conversion using a AD8138. It is powered by 3.3V and the AD9601 is a 1.8V part.

 

Thanks,

 

Doug Gardner

Outcomes