AnsweredAssumed Answered

For ADM809L,  what will the output voltage on RESET pin be when it is sourcing a higher current, like 5mA or 10mA?

Question asked by LarryD on Jul 8, 2016
Latest reply on Jul 11, 2016 by Ren

The ADM809L datasheet specifies the maximum output current of RESET pin is 20mA.  So I assume it is safe to source 10mA for RESET pin.  I want to use this pin to drive an opto-coupler which need  several mA driving current. 

 

The datasheet only specifies the RESET pin output voltage high when sourcing 800uA current. 

Could anyone pls advice what the output voltage on RESET pin will be when it is sourcing a 5mA or 10mA current?   A curve/chart showing the output voltage vs. sourcing current or something similar will be highly appreciated.  thanks.

 

 

Larry

Outcomes