AnsweredAssumed Answered

Configuring Sound Card in BeagleBone Black with ADAU1761

Question asked by vidhya on Jul 7, 2016
Latest reply on Jun 15, 2017 by xabby76

I am trying to integrate the ADAU1761 codec with the Beaglebone Black. I need to configure a sound card in order to play audio through the codec. I tried writing device tree overlay but did not succeed. Then I tried changing directly in the device tree. Now the modes of the PINS are changed but the sound card is not getting configured.

am I going in the right direction? Please help.

 

Below are the changes I made in the device tree:

Pins mode change i2c:

pinmux_i2c2_pins { 
     pinctrl-single,pins = <0x178 0x0b 0x17c 0x0b>;
     linux,phandle = <0x30>;
     phandle = <0x30>;

Pins mode change i2s: 

 mcasp0_pins { 
     pinctrl-single,pins = <0x1ac 0x08 0x19c 0x2 0x194 0x08
     0x190 0x08 0x6c 0x7 0x198 0x08>;
     linux,phandle = <0x47>;
     phandle = <0x47>; };

Driver loading:

i2c@4819c000 { 
     compatible = "ti,omap4-i2c";
     #address-cells = <0x1>;
     #size-cells = <0x0>;
     ti,hwmods = "i2c3";
     reg = <0x4819c000 0x1000>;
     interrupts = <0x1e>;
     status = "okay";
     pinctrl-names = "default";
     pinctrl-0 = <0x30>;
     clock-frequency = <0x186a0>;
     linux,phandle = <0x9d>; phandle = <0x9d>;

     adau1761: adau1361@38 {
          compatible = "adi,adau1761";
          reg = <0x38>;
     };

Sound Card: 

sound { 
compatible = "adi,adau1761-evm-audio";
ti,model = "ADI ADAU1761";
ti,audio-codec = <&adau1761>;
ti,mcasp-controller = <0x52>;
ti,audio-routing =
"Headphone Jack",       "LOUT",
"Headphone Jack",       "ROUT",
"LINE1L",               "LAUX",
"LINE1R",               "RAUX";
clocks = <0x53>;
clock-names = "mclk"; };

Outcomes