AnsweredAssumed Answered

Problem if I modify a Sample Code

Question asked by SteMMo on Jul 6, 2016
Latest reply on Aug 26, 2016 by Kader.M

Hi everyone,

I own the EZBoard Lite for 21489.

I created a project starting from a standard example: adsp-21489-CCES

I modified it to include the schematic and the parameters, following a well known article.

Now I'd like to add some 'actions', then I added a call to initialize the push buttons (InitPushButton(pAppInfo);) in the main() function.

But wherever I put it I receive an unrecoverable error:

 

  A non-recoverable error or exception has occurred.

  Description:   No dispatched handler available for the specified interrupt code.

  General Type:  RunTimeError

  Specific Type: NoDispatchedHandler

  Error PC:      0x001285ba

 

always right after that call.

I moved it in some different points of the main() function but always the same result.

 

My guess was that the call was correct and working ..

How can i solve?

 

Edit: how can i know which interrupt was fired?

Outcomes