AnsweredAssumed Answered

Booting ADSP TS 201S TIGER SHARC FROM EXTERNAL FLASH

Question asked by mohituee on Aug 1, 2011
Latest reply on Aug 8, 2011 by AndyC

Hi

I am working on a project with three ADSP 201S in mutiprocessing mode. I need to boot them one by one from external flash memory.I want to know if the maximum memory size that will be supported is 16 MB for each DSP or combined for all the DSPs.

Also, I want to know

1. The size of the code that would be required to boot each of the three with different code and data respectively.

2. The interfacing requirements.

3. Whether Visual DSP supports only specific flash memories for programming the boot flash memory.

4.I want to use the asynchronous read mode for reading the flash.Is there anything else I need to take care of?

 

Any help on the above would be appreciated.

 

Thanks.

 

Mohit

Bitmapper Integration Technologies.

Outcomes