AnsweredAssumed Answered

ADV7842 L14 pin(HS-IN1) for Conponent YCbCr Video Csync Use

Question asked by Fermat on Jul 1, 2016
Latest reply on Jul 4, 2016 by JeyasudhaMuthuPerumal

Hi

Can ADV7842 L14 pin use for Component YCbCr Video mode sync input.

I use the AIN1,2,3 for Component YCbCr, and L14(HS-IN1) for Csync, but it's not work. No H,V output.

 

The Spec says the L14 is "HS on Graphics Port 1" use.

 

Can thin pin use in component mode Csync, or Should I need connect to SYNC1,2... .

 

Thanks

Outcomes