AnsweredAssumed Answered

Optional Analog Input Pins - Recommended Connector and MatLab

Question asked by ricksturdivant@gmail.com on Jun 30, 2016
Latest reply on Jun 30, 2016 by dmercer

I want to use the two additional analog input pins--the ones that are dedicated analog inputs. Two questions:

1) Do you have a recommended connector for those two optional analog inputs? The pitch does not conform to the 0.1" of the other pins and the through hole is much larger too.

2) Do you have an example MatLab Code examples for capturing data from those two additional analog pints?

 

Thanks,

Rick

Outcomes