AnsweredAssumed Answered

Problem using additional program memory (Aduc 7026)

Question asked by hauke on Aug 1, 2011
Latest reply on Aug 1, 2011 by MMA

Hi,

I am using the Aduc7026 and need more program memory than the internal 62K. This raises a number of questions:

1. Is it possible to download code to external flash memory via Uart, and, if so, can this be done with the ARMWSD utility?

2. Can I use the default bootloader of the Aduc7026?

3. Is a special type of flash memory required, or do certain types make the task of flashing the program code simpler?

Thank you in advance,

hauke

Outcomes