AnsweredAssumed Answered

Qestions about AD8138

Question asked by Tarzan on Jun 27, 2016
Latest reply on Feb 2, 2017 by JinoL

Hi there, I have some questions about AD8138.

 

#1, Is there any problem if this device is  used with V+=7V, V-=-3V?

I checked the simulation tool and I think it looks fine.

 

#2, If the V supply condition is a bit different from the datasheet specification table,

Can I consider the spec of the input voltage range and output voltage swing is the same?

 

#3,I can't find the open loop spec and open loop phase graph. Could you share the data and graph to consider the gain setting and stability?

 

Best regards,

Tarzan

Outcomes