AnsweredAssumed Answered

AD2410 Evaluation kit Selfboot possible?

Question asked by mamsadegh on Jun 23, 2016

Hello every one,

 

we have a AD2410 A2B Bus evaluation kit which basically contains 3 boards, one master node with ADAU1452 on it and two other slave nodes with AD2410.

 

Now I have realized a system for these boards, using sigmastudio and usb cable I can put the design on the boards and it works well.

 

Now I want this evaluation kit to operate in standalone or better to say selfboot mode.

 

According to other posts in this forum, when the master is not in selfboot mode and i have tested the systam and i am sure it works fine, I open the hardware configuration tab,

then I right click on ADAU1452 and select

Self boot memory -- Write lastest compilation through DSP

 

the write oparation gets finished fine.

The check of data also gets finished fine.

 

Now, if I change the DIP switch and put the master board in selfboot mode,

and turn on the boards, Nothing happens.

 

Does any one know why?

 

Thanks

regards

Outcomes