AnsweredAssumed Answered

Error running an app from CrossCore

Question asked by SteMMo on Jun 23, 2016
Latest reply on Jun 30, 2016 by SteMMo

Hi all,

I wrote a sample app starting from the 'UART Echo Back' source for the 21489 EzBoard.

Starting it from VisualDSP I have no problem.

Then I moved into the CrossCore Embedded Studio, defining a debug configuration and changing the interrupt() function with the adi_int_InstallHandler() calls.

If I launch the app I receive he following fatal_error:

 

A non-recoverable error or exception has occurred.

  Description:   No dispatched handler available for the specified interrupt code.

  General Type:  RunTimeError

  Specific Type: NoDispatchedHandler

  Error PC:      0x00124446

 

Which is the 'specified interrupt' ?

If I run the step-by-step mode I do not have the error

 

Any idea?

 

PS: i modified the code that configure a couple of GPIOs as input pins since they are connected with buttons.

I used the code 'Configure a GPIO input' i found among the installed examples.

It uses some adi_gpio_* functions that doesn't exist for 21489.

Outcomes