AnsweredAssumed Answered

SPI problem with FMCOMMS5

Question asked by djog on Jun 23, 2016
Latest reply on Jul 7, 2016 by DragosB

Hi,

I'm working on the KC705 with FMCOMMS5 boards. I'm using the No-os software for AD9361 IC's.

My problem is simple, I can drive one of the two AD9361 but I can't drive the other one.

I can't activate the SPI_ENB_B when i would like to communicate with the AD9361_B.

 

For information, in config.h i activate :

                                                                 #define CONSOLE_COMMANDS

                                                                 #define XILINX_PLATFORM

                                                                 #define FMCOMMS5

 

But i always transmit command to the AD9361_A. I can't understand that.

 

How can I activate the SPI_ENB_B ?

 

Thank you in advance.

Outcomes