AnsweredAssumed Answered

ADA4522 CMRR spec

Question asked by splin on Jun 22, 2016
Latest reply on Jun 23, 2016 by harryh

In the datasheet rev D, CMRR is specified as 155dB typical @ 5V and 160dB for 30V operation, yet figure 30 shows it to be only 110dB from 10Hz to 100Hz, declining thereafter. Presumably the graph is in error?

 

Is CMRR normally specified at DC?

Outcomes