AnsweredAssumed Answered

OpenLDI Clock Rate for ADV7613

Question asked by rpmarchand Employee on Jun 20, 2016
Latest reply on Jul 5, 2016 by edo


Hello,

 

i'm looking to use the ADV7613 to interface with an FPGA for a design and i'm looking to understand the output clock rate on the OpenLDI bus.  From the datasheet i can see that it is operating between 25MHz and 92MHz but i was looking to understand how that relates back to the input clock rate on the HDMI interface. 

 

For example, is 1080p at 147MHz what is the output clock rate?

 

Thanks!

Outcomes