AnsweredAssumed Answered

[Bug Report] Scripting: Delay block - can't change MAX to larger value

Question asked by Vit on Jun 16, 2016

The following script command will modify MAX delay samples value only if new value is lower than existing one:

res = ss.ObjectSetProperties("setControlValue", delay_1_name, 0, 0, "DelaySamples`max", 20 );

 

ADAU1701

 

Tried in SS 3.12 and 3.13beta build1.

 

OS is Windows XP

 

Sample project with script and error message picture are attached

 

Vit

Outcomes