AnsweredAssumed Answered

gain tables

Question asked by rgetz Employee on Jun 13, 2016
Latest reply on Jun 14, 2016 by tlili

In the manual:

http://www.analog.com/media/en/technical-documentation/user-guides/AD9361_Reference_Manual_UG-570.pdf

 

table Table 28. Mixer Gm Gain vs. Index 

indicates "3 − 15 = Index + 11"

 

If my math is correct - an index of 4 should be a gain of 15. (4 + 11)

 

However - Gain Tables in .csv format the 800 MHz table lists index 4 as a gain of 14 (index + 10). Is the table wrong, or is the doc wrong? or is the doc just not detailed enough, and this is actually frequency dependent?

 

Thanks

-Robin

 

  

414

Outcomes