AnsweredAssumed Answered

AD7682 Bipolar Differential Mode

Question asked by jfisherhr on Jul 25, 2011
Latest reply on Jul 27, 2011 by maithil

Hi there,

 

I'm trying to use an AD7682 to sample a differential sensor signal and am seeing some strange results. If I sample IN0 and IN1 separately as single-ended inputs and subtract the two, I get a nice clean signal. If I try using the bipolar differential option, though, I see a steady-state offset as well as some periodic high-frequency noise on the order of about 10 mV (RMS noise using the single-ended option is typically around 0.5 mV).

 

Any ideas what could cause something like this?

 

Updated: Added a chunk of our schematic.

Attachments

Outcomes