AnsweredAssumed Answered

What is the switching speed from RX1A to RX1B?

Question asked by D-Tech on Jun 12, 2016
Latest reply on Jun 27, 2016 by Vinod

I will be using the reference HDL and No-OS drivers. It looks like it is just one register write. If I am not switching rx frequency, will I have to run any recalibrations? Will I have to use 2 fast-lock profiles?

 

Also, do I have any hope of being able to figure out the relative phase relationship between data from RX1B and RX1A after I switch ports? I was hoping I could figure out the max time it would take to do the SPI writes to change the RX input port add some buffer time to that and use that number for a counter in the HDL portion. 

Outcomes