AnsweredAssumed Answered

Synchronization of Multiple AD9959

Question asked by Jiwon.Lee on Jun 10, 2016
Latest reply on Jun 23, 2016 by JLKeip

Hi,

 

I'm trying to design a synchorized multi signal generator based on the figure25 of AD9959 data sheet.

 

1) Can I get detail schematic diagram of this configuration ? Especially between AD9510 and AD9959.

     Want to know which outputs(AD9516) are connected to SLAVE(SYNC_IN) pins.

2-1) Instead of AD9510, Can I use HMC7043 ?

       Because AD9959s are distributed in a few boards. So, want to control output time delay of each SYNC_IN.

2-2) One thing to check in HMC7043, Minimum clock input frequency of HMC7034 is 200MHz.

       Can I use CLKIN port as a SYNC_OUT and CLKOUT ports as a SYNC_INs ?

 

Thanks a lot.

Outcomes