AnsweredAssumed Answered

AD8366: input/output matching networks

Question asked by luca.banchi on Jun 9, 2016
Latest reply on Jul 20, 2016 by ScottH

Dear support,

 

in my design I would adopt the AD8366 DVGA.

I want to ask a reference design or some guide lines in order to match the output and input of the AD8366 with the rest of the circuit:

- on the INPUT the signal is a 50Ohms single-ended.

- on the OUTPUT the AD8366 is connected to an ADC by mean of a twinax 100Ohms cable.

 

Could you please suggest the right matching solution for the AD8366 input and output?

Thank you in advance

Luca

Outcomes