AnsweredAssumed Answered

Need IBIS model for AD9361 with  single ended CMOS 1.8V interface

Question asked by dhar_123 on Jun 7, 2016
Latest reply on Jun 7, 2016 by dhar_123

Hi,

 

I am using AD9361 as a driver in my design. with single ended CMOS 1.8V interface. But, when I simulate the data or clock signals with AD9361 as driver, I get the driver impedence as 96 ohms(which is the impedence for differential signals) which should be around 17.1 ohms approx for single ended signals.

 

I have attached the ibis model(ad9361_1p8_cmos_r2) that i have used for SI simulation.

 

Can you provide ibis model for AD9361 which can be used for single ended signals with interface being CMOS 1.8V?

 

AD9361.PNG

 

 

Thanks & Regards,

Dharitri

Outcomes